DOCA0151EN-03

Firmware Version 8.0.14

Bugs Fixed

  • PowerTag energy sensors connected to PowerTag Link/PowerTag Link HD gateways with firmware version ≥001.006.007 were not visible in FDM128 display.

  • In Device view, the value of current (A) in PowerTag devices was not clearly visible for Russian language.

  • The details of Alarm history for circuit breaker devices were not displayed after navigating from the PowerTag device.

  • Misalignment of display text and translation issues were existing for Chinese, Russian, and French languages.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?