Firmware Version 6.4.2
New Features
- 
                  
Integrated the following devices:
- 
                        
Acti 9 Smartlink SI D gateway
 - 
                        
Enerlin’X IFM Modbus-SL interface
 
 - 
                        
 - 
                  
For MicroLogic X control unit:
- 
                        
Integrated MTZ active alarms and alarm history
 
 - 
                        
 
Bugs Fixed
- 
                  
In the General view grid, toggling of intermittent communication status resulted in unhealthy status, which is indicated in orange.
 - 
                  
Auto-discovery did not always function when more than nine Modbus slave devices were connected to the same master gateway.
 - 
                  
When IO modules were connected to a ComPact NSX circuit breaker without a BSCM installed, the Quick view circuit breaker status was shown as Open.
 - 
                  
For ComPact NSX circuit breaker without a BSCM installed, some pages in Quick view display were shown as Not Responding in the title bar.
 - 
                  
For MasterPact MTZ circuit breaker, FDM128 displayed incorrect contact wear value in maintenance page.
 - 
                  
For MasterPact MTZ circuit breaker, FDM128 displayed incorrect power factor value in measures page.