FDM128 Ethernet Display for Eight Devices
The FDM128 Ethernet display for eight devices (LV434128) is a 1-to-8 human machine interface (HMI). The main component is a 5.7-inch touchscreen.
An FDM128 display can be connected to devices via an Ethernet interface by using any of the following options:
- 
                  
One or more Ethernet gateways (IFE server, Link150, PowerLogic EGX300 and EGX100, PowerTag Link, PowerTag Link B, PowerTag Link HD, Smartlink SI B, or Smartlink Ethernet).
 - 
                  
One or more third-party Ethernet gateways that possess the appropriate characteristics.
 
The FDM128 display monitors and controls up to eight devices from the following list:
- 
                  
Circuit breakers equipped with communicating MicroLogic trip units, such as:
- 
                        
MasterPact MTZ circuit breakers
 - 
                        
MasterPact NT/NW circuit breakers
 - 
                        
ComPact NS circuit breakers
 - 
                        
ComPact NSX circuit breakers
 - 
                        
PowerPact P- and R-frame circuit breakers
 - 
                        
PowerPact H-, J-, and L-frame circuit breakers
 
 - 
                        
 - 
                  
Switch-disconnectors, such as:
- 
                        
MasterPact NT HA switch-disconnectors
 - 
                        
MasterPact NW NA/HA/HA10/HF switch-disconnectors
 - 
                        
ComPact NS NA switch-disconnectors
 - 
                        
ComPact NSX NA switch-disconnectors
 - 
                        
PowerPact P- and R-frame switch-disconnectors
 - 
                        
PowerPact H-, J-, and L-frame switch-disconnectors
 
 - 
                        
 - 
                  
PowerTag Link devices, such as:
- 
                        
PowerTag Link
 - 
                        
PowerTag Link B
 - 
                        
PowerTag Link HD
 
 - 
                        
 - 
                  
Smartlink devices, such as:
- 
                        
Smartlink SI B gateway
 - 
                        
Smartlink Modbus gateway
 
 - 
                        
 
The information displayed includes measures, alarms, and operating assistance data.