990-9000001-001

Connect the Cables between the SMPS AC/DC Converter and the Battery Cabinets

NOTE: One SMPS AC/DC converter can supply up to 10 battery cabinets.
  1. On all the battery cabinets: Disconnect cable 0W76923 from port DC OUT 1 and port DC IN 1 on the SMPS/BMS box. Remove the cable tie from the cable bundle and discard the loose cable 0W76923.
    NOTE: Do not disconnect the other 0W76923 cable from port DC OUT 2 and port DC IN 2 on the SMPS/BMS box.

    The Battery Cabinet

  2. In battery cabinet 1: Route the preinstalled cable 0W13817 from the SMPS AC/DC converter into battery cabinet 1.

    Front View of Battery Cabinet 1

  3. In battery cabinet 1: Connect cable 0W13817 to the connector on the provided cable 0W13819 pin 1 and pin 2.

    Cable 0W13819

    Battery Cabinet 1

  4. In battery cabinet 1: Connect the provided cable 0W13819 to port DC OUT 1 and port DC IN 1 in the SMPS/BMS box as shown above.
  5. For more than one battery cabinet: In battery cabinet 1, connect the provided cable 0W13818 to the connector on the provided cable 0W13819 pin 4 and pin 5. Route cable 0W13818 through the side of battery cabinet 1 into battery cabinet 2.
  6. In battery cabinet 2: Connect cable 0W13818 to the provided cable 0W13819 with the connector on pin 1 and pin 2.

    Battery Cabinet 2

  7. In battery cabinet 2: Connect the cable 0W13819 to port DC OUT 1 and port DC IN 1 in the SMPS/BMS box.
  8. For more battery cabinets: Repeat steps 5,6,7 for battery cabinet 3-10 (up to 10 battery cabinets in the daisy chain).
  9. Optional: In the last battery cabinet in the daisy chain: Connect a cable (not provided) between the last battery cabinet and the SMPS AC/DC converter. The connection is optional, but recommended for improved connection stability.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?