Installation Procedure
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The SMPS AC/DC converter must not be installed in an existing battery cabinet installation.
The SMPS AC/DC converter must be installed before the DC power cables and the battery
module busbars are installed/connected in the battery cabinet.
Failure to follow these instructions will result in death or serious injury.
|
- Follow the battery cabinet installation manual to:
- Prepare the battery cabinet for installation.
- Install seismic anchoring (if applicable).
- Position and interconnect the battery cabinet(s).
- Install the SMPS AC/DC Converter on Battery Cabinet 1.
- Prepare Battery Cabinet 2-10 for Installation.
- Connect the Cables between the SMPS AC/DC Converter and the Battery Cabinets.
- Follow the battery cabinet installation manual to complete the rest of the battery cabinet installation.
- Final Installation.
DANGER