990-9000001-001

Prepare Battery Cabinet 2-10 for Installation

This procedure is performed on battery cabinets 2-10.
  1. Lockout/Tagout the battery breaker in the open (OFF) position.
  2. Remove the indicated cover.
  3. Open the two fuse holders (P-IN and B-IN).
  4. Remove the P-IN fuse from the fuse holder.
  5. Loosen the two screws from the SMPS/BMS box and pull out the SMPS/BMS box enough to disconnect it. Do not pull out the SMPS/BMS box completely.
  6. Remove the two top plates.
  7. Disconnect the internal cable 0W76922 from the P+ busbar. Reinstall the nut on the P+ busbar.

    Top View of the Battery Cabinet

  8. Disconnect the internal cable 0W13501 from the P- busbar. Reinstall the nut on the P- busbar.
  9. Remove the cable lugs from the two internal cables 0W76922 and 0W13501 and terminate the cables into a connector (not provided). Fasten the connector to the one of the bridges with the provided cable ties. Recommended connector type to use is Phoenix 1757022 or a three-pin connector with similar specifications (see table below).
    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Terminate the two internal cables 0W76922 and 0W13501 into a three-pin connector to reduce risk of short circuit. Keep the middle pin empty.
    Failure to follow these instructions will result in death or serious injury.

    Phoenix 1757022 Connector Specifications

    Rated current 12 A
    Rated voltage(III/2) 320 V
    Number of positions 3
    Pitch 5.08 mm
    Wire 20 AWG
  10. Reinstall the two top plates on the battery cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?