990-9000001-001

Final Installation

  1. Push the SMPS/BMS box into position and reinstall with the screws on all the battery cabinets.
  2. Close the fuse holders on all the battery cabinets.
    NOTE: The P-IN fuse must NOT be reinstalled.
  3. Reinstall the covers on all the battery cabinets.
  4. Connect the AC input cable (not provided) to the AC/DC converter(s). The AC input can be supplied from the UPS or from another AC source. Inlet on AC/DC converter is C20 Schurter 4798. Required mating connector on AC input cable is C19 Schurter 4795.
    NOTE: A fuse is assembled inside the AC/DC converter for AC input protection. Fuse holder: 2P, for 10 x 38 mm fuse. Fuse rating: 10 A 500 VAC, 120 kA interrupting.

    Battery Cabinet 1

Refer to the operation manual for start-up of the battery cabinet(s).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?