990-5937G-001

Environment

  Operating Storage
Temperature -10 °C to 40 °C (14 °F to 104 °F) -25 °C to 55 °C (-13 °F to 131 °F)
Relative humidity 10 to 70% non-condensing 10 to 90% non-condensing
Elevation 0 m to 2011 m (0 feet to 6600 feet) above sea level
152 m below to 7620 m above sea level
(500 feet below to 25,000 feet above sea level)
Protection class NEMA type 1, solid roof, external doors with inner dead front panels
Cooling Front and rear ventilation (top and bottom)
Color

RAL 9003 white and APC raven black

Accessibility Front access for:
  • Display

  • Fuse panel

  • Communication and monitoring

  • Adding/replacing branch breakers

Heat Dissipation

Commercial reference PMM400-ALAX
PMM400-ALA
PMM400-CUB PMM500-ALAX
PMM500-ALA
PMM500-CUB
kVA 400 500
Heat dissipation in BTU/hr 16018 14592 20616 18450
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?