990-5937H-001

Model List

400 kVA PDU

  • 400 kVA Galaxy PDU with aluminum transformer with limited configurable options (PMM400-ALAX)

  • 400 kVA Galaxy PDU with aluminum transformer with a wide range of configurable options (PMM400-ALA)

  • 400 kVA Galaxy PDU with copper transformer with a wide range of configurable options (PMM400-CUB)

500 kVA PDU

  • 500 kVA Galaxy PDU with aluminum transformer with limited configurable options (PMM500-ALAX)

  • 500 kVA Galaxy PDU with aluminum transformer with a wide range of configurable options (PMM500-ALA)

  • 500 kVA Galaxy PDU with copper transformer with a wide range of configurable options (PMM500-CUB)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?