990-91735-001

Compliance

Safety IEC 61010-1:2010/AM1:2016 3.1 edition 2017-01 Safety requirements for electrical equipment for measurement, control, and laboratory use
IEC 61010-2-201: 2017 2nd edition 2017-3 Safety requirements for electrical equipment for measurement, control, and laboratory use
UL 1778, UNINTERRUPTIBLE POWER SYSTEMS, Edition 5, Revision Date 10/12/2017
CSA C22.2 No. 107.3, UNINTERRUPTIBLE POWER SYSTEMS, Edition 3, Revision Date 10/12/2017
EMC/EMI/RFI EN/IEC 61000-6-4:2018 Emission standard for industrial environments
EN/IEC 61000-6-2:2016 Immunity standard for industrial environments
Earthing system TN, TT, IT
Overvoltage category OVCII
Pollution degree 2
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?