990-91735-001

Prepare the Remote Centralized Display for Cables

  1. Remove the bottom gland plate.

    Front Bottom View of the Remote Centralized Display

  2. Drill or punch holes for power cables and signal cables in the bottom gland plate.

    For PG20 and 1/2 inch conduit, drill ø20 mm (0.79 in) hole.

    For PG32 and 1 inch conduit, drill ø32 mm (1.26 in) hole.

    Bottom Gland Plate

    NOTE: Use conduits and glands that fit to the cable size going in/out of the remote centralized display. Conduit should be certified according UL514B, DWTT/7 or equivalent. Use M20 and M32 glands from LAPP GmbH (53111020, 6-13 mm diameter and 53111040, 9-21 mm diameter) certified to IEC 50262,VDE135320 or equivalent.
  3. Reinstall the bottom gland plate.

    Front Bottom View of the Remote Centralized Display

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?