990-91735-001

Recommended Cable Sizes

DANGER
hazard of electric shock, explosion, or arc flash
All wiring must comply with all applicable national and/or electrical codes.
Failure to follow these instructions will result in death or serious injury.
NOTE: Overcurrent protection is to be provided by others.
  • Copper cable, maximum cable diameter: 12 AWG or 4 mm2, minimum cable diameter: 16 AWG or 1.5 mm2

  • Minimum 75 °C (167 °F) conductors

  • An ambient temperature of 30 °C (86 °F)

  • Use of copper conductors

  • A readily accessible disconnection device shall be incorporated externally to the system and disconnect from all current carrying conductors.

  • Input cable connection with cable glands is allowed for NFPA79 application only

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?