990-91735-001

Remote Centralized Display Specifications

The remote centralized display (GVLOPT007) offers the ability to monitor and control up to 6 UPSs in parallel from a single point.

  • Centralized monitoring of up to 6 UPSs

  • Centralized synchronized transfer command (Inverter – Bypass)

  • External breaker monitoring through PLC

Display 10 inch Magelis Display HMIST6500
Connection to UPS CAT 5e SF/UTP
Input voltage 380 V, 400 V, 415 V, 440 V, 480 V
Input frequency 50/60 Hz
Connections 3PH + PE
Maximum input current 70 mA
Maximum upstream circuit breaker 20 A
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?