990-91735-001

Mimic Diagram

The home screen shows the mimic diagrams for parallel systems. Tap on each UPS to see the mimic diagram on UPS level.

The mimic diagram will adapt to your system configuration – the mimic diagrams shown here are just examples.

Example of Mimic Diagram on UPS Level

The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.

NOTE: The mimic diagram only shows one battery breaker BB even if more battery breakers have been connected and configured for monitoring. If one or more of the monitored battery breakers are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery breakers are in the open position, the BB on the mimic diagram will show as open.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?