990-91315B-001

Prepare the Maintenance Bypass Panel for Cables

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the maintenance bypass panel.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the gland plate.
  2. Drill or punch holes for cables or grommets in the gland plate.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.
  3. Install grommets (if applicable) and reinstall the gland plate.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?