990-91315B-001

Connect the Power Cables

  1. Remove the cover from the PE busbar.
  2. Connect the PE cables to the PE busbar.
  3. Reinstall the cover on the PE busbar.
  4. Do one of the following:
    • For single mains: Connect the input cables from utility/mains.
    • For dual mains: Connect the bypass cables from utility/mains.
  5. Do one of the following:
    • For single mains: Connect the UPS input cables.
    • For dual mains: Connect the UPS bypass cables.
  6. Connect the UPS output cables.
  7. Connect the load cables.
  8. Fasten the cables with cable ties (not provided) to the cable reliefs in the left side, top, and bottom of the maintenance bypass panel.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.