990-91315B-001

Remove the Neutral Jumpers

NOTE: The neutral jumper makes a bolted connection of the neutral so that the neutral is not disconnected when the 4-pole breakers are opened.
NOTE: Only remove the neutral jumpers in a Galaxy VS installation, if this is a local requirement. Removal of the neutral jumpers is an option for a Galaxy VS installation.
NOTE: Always remove the neutral jumpers in an Easy UPS 3M installation. Removal of the neutral jumpers is mandatory for an Easy UPS 3M installation.
  1. Remove the neutral jumpers from the breakers.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.