990-91315B-001

Connect the Signal Cables for the Galaxy VS UPS

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.
  1. Connect the Class 2/SELV signal cables for the breaker indicator lights from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.
    NOTE: The breaker indicator light circuit is considered Class 2/SELV. Class 2/SELV circuits must be isolated from the primary circuitry. Do not connect any circuit to the breaker indicator light terminals unless it can be confirmed that the circuit is Class 2/SELV.
  2. Connect the non-Class 2/non-SELV signal cables from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.

    Single Mains

    Dual Mains

  3. Pull up the slack in the signal cables and fasten the signal cables to the cable reliefs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.