990-91261E-001

Install the Seismic Anchoring (Option)

  1. Mount the rear anchor(s) to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchor is ø14 mm.
  2. Install the rear anchoring bracket on the UPS with the provided M8 bolts.

    Rear View of the UPS

  3. Install the seismic front anchoring bracket on the UPS with the provided M8 bolts.

    Front View of the UPS

    NOTE: Do not push the UPS into position yet.
QR code for this page

Was this helpful?