990-91261G-001

Connect the Signal Cables from a Modular Battery Cabinet

  1. Route the signal cables from modular battery cabinet 1 through the left side of the UPS (for an adjacent modular battery cabinet) or through the rear of the UPS (for a remote modular battery cabinet).

    Front View of Adjacent Modular Battery Cabinet 1 and the UPS

  2. Connect the signal cables from modular battery cabinet 1 to the UPS:
    1. Disconnect the termination plug from J8008 on board 640-7552 in the UPS.
    2. Mount the termination plug in J8008 on board 640-7552 in the last modular battery cabinet (T).
    3. Connect the signal cable from J8011 on board 640-7552 in modular battery cabinet 1 to J8014 on board 640-7552 in the UPS.
    4. Connect the signal cable from J8007 on board 640-7552 in modular battery cabinet 1 to J8008 on board 640-7552 in the UPS.
    Modular Battery Cabinet 2,3,4 Modular Battery Cabinet 1 UPS
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?