990-91261G-001

Galaxy VSUPS with Up to 4 Internal Battery StringsInstallation

10-50 kW 400 V
20-50 kW 480 V
10-25 kW 208 V

Latest updates are available on the Schneider Electric website

5/2025

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?