990-55224-001

Configure the Network

The network can be configured for the integrated and the optional network management card (NMC).

  1. Tap Configuration > Network > IPv4 and select Integrated NMC to configure the integrated network management card or Optional NMC to configure the optional network management card.
    1. Set the Address mode to Manual, BOOTP, or DCHP.
    2. You can also disable the network by selecting Disable integrated NMC IPv4/Disable optional NMC IPv4.
    3. Tap OK to save your settings.
  2. Tap Configuration > Network > IPv6 and select Integrated NMC to configure the integrated network management card or Optional NMC to configure the optional network management card.
    1. Set the DHCPV6 mode to Address and other information, Non-address information only, or IPv6 never.
    2. Select Auto configuration or Manual.
    3. You can also disable the network by selecting Disable integrated NMC IPv6/Disable optional NMC IPv6.
    4. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?