990-55224-001

Save the UPS Settings on a USB Device

NOTE: The UPS can only accept settings that were originally saved from the same UPS. Settings saved from other UPSs can not be reused.
  1. Tap Configuration > Save/restore.
  2. Open the front panel.
  3. Insert your USB device in USB port 1 on the UPS.
  4. Tap Save to save the present UPS settings on the USB device.
    NOTE: Do not remove the USB device until the save process has finished.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.