990-55224-001

Turn the Inverter OFF

IMPORTANT: This will turn off the supply to the load.
  1. Select Control > Inverter > Inverter off.
  2. Tap OK on the confirmation screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?