990-91140H-001

Heat Dissipation for Maintenance Bypass Cabinet with Transformer in BTU/hr

  Maintenance bypass cabinet with input transformer Maintenance bypass cabinet with output transformer
Commercial reference GVSBPIT25B GVSBPIT50 GVSBPIT75 GVSBPOT50B GVSBPOT100 GVSBPOT150
100% load 2700 5300 8000 5300 10600 16000
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.