990-91264A-001

Connect the Signal Cables

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.

Bottom Cable Entry System

Top Cable Entry System

  1. Connect the Class 2/SELV signal cables for the breaker indicator lights from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.
    NOTE: The breaker indicator light circuit is considered Class 2/SELV. Class 2/SELV circuits must be isolated from the primary circuitry. Do not connect any circuit to the breaker indicator light terminals unless it can be confirmed that the circuit is Class 2/SELV.

    Single Mains System

    Dual Mains System

  2. Connect the non-Class 2/non-SELV signal cables from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.
    NOTE: Only for GVSBPSU60G-WP: Terminal 11 and 12 are not present on the control terminal block in GVSBPSU60G-WP and there is no connection needed to J6601 in the UPS.

    Single Mains System

    Dual Mains System

  3. Pull up the slack in the signal cables and fasten the signal cables to the cable reliefs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?