Mount the Battery Breaker Box to the Wall
CAUTION |
|---|
|
Risk of injury or equipment damage
Failure to follow these instructions can result in injury or equipment damage.
|
- Measure and mark the four mounting hole locations on the wall.
- Drill holes in each of the four marked locations.
- Open the front door of the battery breaker box.
- Lockout/Tagout the battery breaker in the OFF (open) position.
- Loosen the three screws and open the dead front panel.
- Lift the battery breaker box, position it against the wall
and line it up with the four holes. Fasten with four M10 screws.NOTE: Four M10 x 30 torx and nuts are supplied for mounting the battery breaker box to a battery rack. If the battery breaker box is mounted to a wall, use suitable mounting equipment.
CAUTIONHeavy loadThe battery breaker box is heavy (60 kg). Use appropriate tools to safely lift the battery breaker box.Failure to follow these instructions can result in injury or equipment damage.