990-5456C-001

Installation Procedure

DANGER
hazard of electric shock, explosion or arc flash
Place the battery breaker box as close to the battery bank as possible to limit the length of unprotected battery cable.
Failure to follow these instructions will result in death or serious injury.
NOTE: The maximum distance between the temperature sensor and the battery breaker box is 2.4 m due to the length of the supplied cable.

Overview of Signal Cables and Power Cables for Configuration with Eight Battery Strings

  1. Mount the Battery Breaker Box to the Wall.
  2. Prepare the Battery Breaker Box for Cables.
  3. Connect the Power Cables.
  4. Connect the Signal Cables between the I/O Cabinet and the Battery Breaker Boxes.
  5. Final Installation Steps.
For moving or decommissioning the battery breaker box after installation has been completed, see Decommission or Move the Battery Breaker Box to a New Location.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?