Decommission or Move the Battery Breaker Box to a New Location
- Shut down the UPS completely – follow the instructions in the UPS operation manual.
- Lockout/Tagout all breakers in the switchgear in the OFF (open) position.
- Lockout/Tagout all battery breakers in the switchgear/battery solution in the OFF (open) position.
- For battery solutions with no individual battery breaker
upstream of this battery breaker box, disconnect the battery cables
from the battery solution.
DANGERHazard of electric shock, explosion, or arc flashDisconnect the battery cables from the battery solution.Failure to follow these instructions will result in death or serious injury. - Open the front door of the battery breaker box.
- Lockout/Tagout the battery breaker in the OFF (open) position.
- Loosen the three screws and open the dead front panel.
- Loosen the screw of each inner cover and lift the covers up and out of the battery breaker box.
- Measure for and verify ABSENCE of voltage on each DC busbar before continuing.
- Disconnect and remove all power cables from the battery breaker box.
- Reinstall the inner covers.
- Disconnect and remove all temperature sensor signal cables from the battery breaker box. See Connect the Power Cables for details.
- Disconnect and remove all signal cables from the battery breaker box. See Connect the Signal Cables between the I/O Cabinet and the Battery Breaker Boxes for details.
- Remove the four M10 screws from the wall and remove the
battery breaker box from the wall.
CAUTIONHeavy loadThe battery breaker box is heavy (60 kg). Use appropriate tools to safely lift the battery breaker box.Failure to follow these instructions can result in injury or equipment damage. - Close the dead front panel and fasten with the three screws.
- Close and lock the front door of the battery breaker box.
- For transport:
WARNINGTIPPING hazardFor transport of the battery breaker box ensure:- that personnel performing the transport have necessary skills and have received adequate training;
- to use appropriate tools to safely lift and transport the product;
- to protect the product against damage by using appropriate protection (like wrapping or packaging).
Failure to follow these instructions can result in death, serious injury, or equipment damage.Transportation requirements:
-
Mount the battery breaker box in a horizontal position in the center of a suitable pallet with minimum pallet dimensions: 840 mm x 1220 mm. The pallet must be suitable for the weight of the battery breaker box (60 kg).
-
Mount the battery breaker box to the pallet with appropriate means of fixation that can withstand vibrations and shocks during loading, transport, and unloading.
-
The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.
WARNINGUnexpected equipment behaviorDo not lift the battery breaker box with a forklift/pallet truck directly as it may bend or damage the battery breaker box.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Perform one of the following:
- Decommission the battery breaker box, OR
- Move the battery breaker box to a new location to install it.
- Only for installing the battery breaker box in a new location: Follow the installation manual to install the battery breaker box in the new location. See Installation Procedure for installation overview. Reinstallation and startup must only be performed by qualified personnel.