990-5456C-001

Prepare the Battery Breaker Box for Cables

DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or grommets with the gland plates installed, and do not drill or punch in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the bottom gland plate.

    Front Bottom View of Battery Breaker Box

  2. If the cables from the I/O cabinet should be routed through the top, remove the top gland plate.

    Front View of Battery Breaker Box

  3. Drill or punch holes for cables or grommets (not provided).
  4. Install grommets (if applicable) and refit the gland plate(s).
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.

    Front View of Battery Breaker Box

    Front Bottom View of Battery Breaker Box

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?