8536CT1901

Schematics

Motor Circuit Breakers

 

Add-on auxiliary contacts according to their location

GV5PB/6PB

 

GV7AE11, GV7AB11

   

Location 1
C/O contact

Location 2
Trip indication

Location 3
Electrical fault indication*

Location 4
C/O contact

 

Electric trips

GV7AU

GV7AS

 

Thermal fault module S429424

 
 

Recommended application schematic for S429424

SD1, SD3: thermal fault module input power supply
SD2: overload fault signal output. This output will stay pul until reset.
SD4: contactor control output
SD2 and SD4: static outputs: 24–415 Vac/Vdc; 80 mA maximum
KM1: LC1 D or LC1 F contactor
KA1: CA2 or CAD type control relays
Terminals shown in green must be connected by the customer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?