DOCA0148EN-07

Firmware Version 005.003.000

New Features

  • Enabled ULP communication for MasterPacT MTZ circuit breakers with MicroLogic Active control unit and BCIM module.

  • Enabled data logging and publishing for serial devices connected to IFE server through IFM interface and Modbus SL hub.
  • Added IO MODULES page under MONITORING & CONTROL tab of IFE webpage, where you can view input/output configuration of IO modules connected to the IFE server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.