7DE02-0406-04

Chinesische Normenkonformität

Dieses Produkt erfüllt die folgenden chinesischen Normen:

IEC 61557-9:2014 Electrical safety in low voltage distribution systems up to 1 000 V a.c. and 1 500 V d.c. - Equipment for testing, measuring or monitoring of protective measures - Part 9: Equipment for insulation fault location in IT systems

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

War das hilfreich für Sie?