DOCA0149EN-04

Firmware Version 003.005.001

Bugs Fixed

The breaker operation from IO module was not possible after the firmware upgrade of the BCM ULP module.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?