DOCA0149EN-04

Firmware Version 003.004.005

New Features

Added a new user-defined application: Alarm Indicators, to assign ground-fault alarm and earth-leakage alarm to digital outputs.

Bugs Fixed

  • Digital output state was inconsistent due to the impact of shock and vibration on the output relays.

  • IO module did not respond when IFE server or interface lost the SNTP connection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?