DOCA0149EN-04

IO Module for One Circuit Breaker

The IO input/output application module for one circuit breaker (or IO module) is a part of an ULP system with built-in functionalities and applications.

The ranges of circuit breakers compatible with the IO module are:

  • MasterPacT MTZ circuit breakers

  • MasterPacT NT/NW circuit breakers

  • ComPacT NS circuit breakers

  • ComPacT NSX circuit breakers

  • PowerPacT P- and R-frame circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

The IO module resources are:

  • Six digital inputs that are self-powered for either NO or NC dry contact or pulse counter.

  • Three digital outputs that are bistable relays (5 A maximum).

The predefined applications can be configured using the rotary switch.

The user-defined applications can be configured using the EcoStruxure Power Commission software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?