DOCA0149EN-04

Firmware Version 003.002.002

New Features

Added the compatibility feature with MasterPacT MTZ circuit breakers.

Bugs Fixed

  • The input/output values of the IO module was freezed when the power supply was insufficient.

  • When IO module was powered up with the circuit breaker being in the disconnected position, the cradle status was not reported.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?