DOCA0149EN-04

Firmware Version 003.002.009

New Features

Added a new feature to allow addition of two IO modules in position 9.

Bugs Fixed

IO module was reset to factory settings when exiting from Fallback mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?