Maintenance Menu

Description

The Maintenance menu contains the following submenus:

Level 1

Level 2

Level 3

Function description

Home

Maintenance

Switch to other set(1)

Dual setting configuration

Assistance

Presents information about the maintenance schedule and the firmware version and the hardware version of the MicroLogic X control unit.

Health

Describes the health state of the circuit breaker.

CB overview

Presents information about the circuit breaker.

(1) Displayed only when the parameter Dual settings is set to Enabled and the parameter Switch Mode is set to Local HMI.

Switch to Other Set

The Switch to other set menu is displayed only when the parameter Dual settings is set to Enabled and the parameter Switch Mode is set to Local HMI. It presents the following data:

Level 3

Level 4

Parameter name

Switch to other set

Switch to set B

Selection of the setting group A or B when the dual settings function is enabled.

Assistance

The Assistance menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Assistance

Maint.schedule

Next Maint.

Displays:

  • Next maintenance program to be performed

  • Number of months before program is due, or number of months program is overdue

Last Maint.

Displays:

  • Last maintenance program performed and date

  • Name of maintenance provider

  • Name of maintenance personnel who carried out the program

 

Firmware Version

μLogic version

Displays the MicroLogic X firmware version in the format aaa.bbb.ccc.

M&P version

Displays:

  • M&P firmware version and TCI firmware version, used to check compliance with UL 489SE

  • CRC32 code of the firmware versions

TCI version

ASIC version

Displays the ASIC firmware version.

Measure version

Displays:

  • Firmware version of the measurement algorithm, used to check compliance with IEC 61557-12

  • CRC32 code of the firmware version

 

Hardware Version

HMI version

Displays hardware version of the MicroLogic X embedded display screen.

Health

The Health menu presents the following data:

Level 3

Level 4

Parameter name

Health

Circuit breaker

Displays remaining service life of the breaking block as a percentage

MicroLogic

Displays remaining service life of the MicroLogic X control unit as a percentage

Actuator wear

Displays as a percentage the wear of the following auxiliaries:

  • MCH gear motor

  • XF closing voltage release

  • MN undervoltage release

  • MX1 opening voltage release

  • MX2 opening voltage release

Contact wear

Displays wear of the contacts as a percentage

CB Overview

The CB overview menu presents the following data:

Level 3

Level 4

Parameter name

CB overview

CB block

Circuit breaker range: MasterPacT

Device size: MTZ1, MTZ2, or MTZ3

Rated current x 100 A (Example: 08 corresponds to a rated current In of 800 A)

Performance level: N1, H1, H2, H3, or L1

Power system: 3P or 4P

Standard: IEC, UL, or ANSI

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?