DOCA0102EN-12

Health State

Presentation

The health state of the circuit breaker is determined from the following functions:

The health state of the circuit breaker is represented with one of the following icons:

  • OK (white).

  • Medium severity detected alarm that requires non-urgent action (orange).

  • High severity detected alarm that requires immediate corrective action (red).

For more information, refer to the list of events.

Service LED

The service LED alerts the user to the health state of the circuit breaker:

  • Orange LED: medium severity detected alarm that requires non-urgent maintenance action

  • Red LED: high severity detected alarm that requires immediate maintenance action

Data Availability

The health state indicator with additional details about the health state of the circuit breaker is available as follows:

  • On the MicroLogic X display screen, at: Home > Quick View > Health

  • With EcoStruxure Power Commission software

  • With EcoStruxure Power Device app through Bluetooth or USB OTG connection

  • On a remote controller using the communication network

NOTE: Quick View on the MicroLogic X display screen displays the health state with the OK icon when no high or medium severity event is detected.

When a high or medium severity event is detected a pop-up screen is displayed. If the pop-up is acknowledged by pressing OK, the orange or red icon is displayed again in Quick View scrolling and is available at Home > Quick View > Health if scrolling is disabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.