FAST ZBY2328 FORWARD ZBY2305 FOR-REV ZBY2371 HAND ZBY2316 HAND-OFF-AUTO ZBY2387 INCH ZBY2321 JOG ZBY2382 LEFT ZBY2310 OFF ZBY2312 OFF-ON ZBY2367 ON ZBY2311 OPEN ZBY2313 POWER ON ZBY2326 RESET (red background) ZBY2323 RESET (black background) ZBY2322 REVERSE ZBY2306 RIGHT ZBY2309 RUN ZBY2334 SLOW ZBY2327 START ZBY2303 STOP ZBY2304 STOP-START ZBY2366 UP ZBY2307
Section 16: NEMA and Definite Purpose Contactors and Starters
General Purpose Enclosuresfor Type DP, DPA Contactors Class 8910Type Full Load(A) Poles Class 9991Type DP 30–40 1 & 2 DPG1 DPA 30–40 2 & 3 DPG1 DPA 5030–40 2 & 34 DPG2 DPA 60–75 2 & 3 DPG3 DPA 90 2 & 3 — Terminals Full Load(A) Power Terminals Type of Lug For Ring Tongue, add RT after
RSZ accessories 8501NR45 Socket+8501RS14V20 Relay 8501RS14V14 8501RSD34V51 8501R relays are suited for use as logic elements and power switching output devices. The short stroke motion of the armature provides long mechanical life required for high speed operation of control systems. Different