63249–402–200 Rev. 04

Completing the Installation

  1. Verify that the power supply is installed correctly by noting whether the CL1 and CL2 LEDs are lit. If lit, the power supply was installed correctly.

  2. To allow the power supply to protrude through the panelboard deadfront, remove the twist-outs in the deadfront corresponding with the power supply position.

  3. Proceed with the installation of other panelboard components according to related instruction sheets. When finished with the installation, replace the deadfront and panelboard cover, and turn on the power to the Powerlink system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?