63249–402–200 Rev. 04

Connecting to a Subnetwork

If the NF panelboard is part of a subnetwork, follow these instructions to connect the subnet connector to the power supply.

NOTE: Powerlink power supplies can also be installed in Powerlink remote mount controllers. Refer to 80043–870–01 for more information.

  1. Using the four-wire,18 AWG subnet cable (General Cable 236100, Belden 27326, or equivalent) from the main network, insert one of the colored wires into the first terminal of the subnet connector plug.

    NOTE: If connecting to one or more secondary panelboards, refer to the installation and wiring instruction sheet for the secondary address selector.

    Subnet Connector Plug Wire Installation

  2. Once the wire is in place, secure the terminal by torquing the screw to 5 lb-in. (0.6 N•m).

  3. Using the same process above, secure the wires into the remaining three terminals A, –, and + (see Figure 4).

    NOTE: It is important to use the same wire color sequence for all subnet connector plugs. For example, if a blue wire is inserted into the first terminal for the first subnet connector plug, the blue wire must be inserted into the first terminal on all additional subnet connector plugs.
  4. Push the subnet connector plug into the mating connection on the left side of the power supply (see Figure 5).

    Connecting the Subnet Connector Plug to the Power Supply

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?