63249–402–200 Rev. 04

Connecting to a Controller

Follow these instructions to connect the power supply to the controller. The process is illustrated in Connecting to the Controller.

  1. Install the controller according to the instruction sheet provided with the controller.

  2. Push the power supply connector plug into the power connection on the controller (see Connecting to the Controller).

    NOTE: If a column-width NF panelboard is used, the column-width controller cable NFCWG3 is required to connect the power supply and controller.

    Connecting to the Controller

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?