SUG_Wiser_New_Zealand_WSE-05

Connected dimmers

Wiser Micro Module Dimmer

Enables convenient multi-way switching and dimming by connecting up to 10 compatible momentary push-button switches.

NOTE: Momentary push buttons must be certified for use in 220-240V AC applications. Use for non Iconic wall plates such as Saturn Zen.

Instruction Sheet (PDF)

Device User Guide

Iconic Connected Dimmer — Zigbee default

Controls the lighting level in a room, or automatically sets lighting to a desired level in response to a specified condition or event using the push button.

Use with Iconic, Iconic Styl, Iconic Essence or Pro Series plates.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.