SUG_Wiser_New_Zealand_WSE-05

Device button/key and LED locations

Find the location of buttons, keys and LED indicators on various devices.

Wiser Micro Module Blind

The external push button is also the reset button. See the device instructions for more information.

NOTE: There is no LED indication.

   

Wiser Micro Module Dimmer

The external push button is also the reset button. See the device instructions for more information.

NOTE: There is no LED indication.

Wiser Window/Door Sensor

(See A) Function key

(See B) Status LED (visible on front of master part when flashing or lit)

Wiser Motion Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser Water Leakage Sensor

(See A) Function key

(See B) Status LED (visible on top of sensor when flashing or lit)

Wiser Temperature/Humidity Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser IP Camera Indoor

(See A) Micro SD Card slot

(See B) Status LED

(See C) Reset Button

Wiser Smoke Alarm Lithium Battery Square

(See A) Reset button

(See B) Standby LED

(See C) Status LED

Iconic Connected AC Fan Speed Controller, Zigbee/BLE

See (A) Push-button/Reset button

See (B) Speed indicating LEDs

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.