SUG_Wiser_New_Zealand_WSE-05

Devices with motion sensors

Symptom

Possible cause

Solution

Load does not switch on automatically.

NOTE: This does not apply to the battery-powered .

Detection brightness for the sensor is low.

Increase the detection sensitivity in device settings.

Load does not switch off automatically when an Automation is triggered.

The Automation may include a delay Action that is set too long.

Reduce the Action delay time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.