SUG_Wiser_New_Zealand_WSE-05

Blinds control

Symptom

Solution

Connected blinds cannot be controlled.

  • Check the power supply.

  • Remove power to the blinds control switch and then re-connect power again.

  • Check the load.

  • In the case of an external push button, check the wiring.

  • Re-couple devices.

Blinds is not driving to the desired position.

Re-calibrate the blinds. See Calibrating ShutterBlinds

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.