SUG_Wiser_New_Zealand_WSE-05

Dimmers

Symptom

Solution

Dimming up not possible.

  • Reduce/increase load.

  • Allow the dimmer module to cool in case of overheating.

Switching on not possible.

  • Allow the dimmer module to cool in case of overheating.

  • Reduce load.

  • Change load.

  • Check externally-connected push buttons and joined/paired devices:

    • In the case of an externally-connected push button, check the wiring between the push button and the dimmer.

    • In the case of joined/paired devices, remove the assignments between the devices and re-join.

Brightness level reaches below the default value.

  • Reduce/increase load.

  • Reduce maximum brightness.

Flickering at minimum brightness.

Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device).

Flickering

  • Change load.

  • Set RL LED mode.

  • Reset to default settings if you are using a micro module dimmer.

Only slight dimming capability

  • Install a 31LCDA load correction device

  • Change dimming range.

  • Set RL LED mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.