DOCA0239EN-11

Version 3.0.1

New Features

IO Optimization feature extension to EcoStruxure Machine Expert function blocks library.

Bugs Fixed

  • Voltage Fluctuation Status Reset is not functioning in DIAGNOSTICS power voltage section.

  • Voltage Phase Sequence information is updated incorrectly when there is no voltage supply to Voltage Interface Module (VIM).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?